AXIS#.GEAR.IN

Description

This parameter sets the denominator of the gear ratio for the electronic gearing mode. The gear ratio is used in order to increase and decrease the slave velocity. The slave velocity can be calculated by the following formula:

Slave velocity = Master velocity * AXIS#.GEAR.OUT/AXIS#.GEAR.IN

Be sure that you set the external master source number of signals per revolution correctly. See AXIS#.GEAR.FBSOURCE to determine the gearing master source and verify the feedback resolution for that device.

Versions

Action Version Notes
Implemented 02-00-00-000
     

General Information

This content is not applicable to KAS, using either a PACClosed"Programmable Automation Controller" PAC is a compact controller that combines the features and capabilities of a PC-based control system with that of a typical programmable logic controller (PLC). A PAC thus provides not only the reliability of a PLC, but also the task flexibility and computing power of a PC. Additionally, because they function and communicate over popular network interface protocols, PACs are able to transfer data from the machines they control to other machines and components in a networked control system or a PDMM.

Type

Read/Write

Units

N/A

Range

1 to 65,535

Default Value

1

Data Type

Integer

See Also

N/A

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported

Fieldbus Information

FieldbusClosedA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Parameter Index Sub-Index Data Type Float Scale Units Access PDO Mappable
EtherCATClosedEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen AXIS1.GEAR.IN 0x5006 0x3 UINT - - RW False
AXIS2.GEAR.IN 0x5106 0x3 UINT - - RW False

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen